:SWITch:CONNected?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:SWITch:CONNected?
Query Response
{0 | 1}
Description
Returns 1 if FlexOTO is connected to a switch either by scanning for a recognized switch or by running a user switch driver. Returns 0 if no switch has been detected or installed (with a user driver). To connect the instrument driver, use the :SWITch:RDRiver command.