:SWITch:DISConnect
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:SWITch:DISConnect
Description
Removes a currently recognized switch from the Hardware Diagram. The switch could have been automatically detected or installed with a user switch driver. This command is equivalent to clicking Exit in the Switch Connection Setup dialog.