:SYSTem:ERRor:COUNT?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Query Syntax
:SYSTem:ERRor:COUNT?
Description
Returns the string which is the number of errors contained in the error-message buffer. To return the "first in" error, use the :SYSTem:ERRor:NEXT? query.
Example Python 3.x Script
This script opens a session with FlexOTO running on the PC and sends two invalid commands that create two error messages. FlexOTO's error buffer is then queried for the errors.
import visa # import VISA library rm = visa.ResourceManager() FlexOTO = rm.open_resource('TCPIP0::localhost::hislip0,4880::INSTR') #HiSLIP FlexOTO.timeout = 20000 # Set connection timeout to 20s FlexOTO.read_termination = '\n' FlexOTO.write(':HAPPY:BIRTHDAY TODAY') # Illegal command for error! FlexOTO.write(':TIMebase:POSition 2.4E10') # out of range for error! error_cnt = int(FlexOTO.query(':SYSTEM:ERRor:COUNt?')) if error_cnt == 0: print('\n\tNo FlexOTO errors reported.') else: for i in range(0,error_cnt): print('\tERROR: ' + FlexOTO.query(':SYSTem:ERRor:NEXT?')) FlexOTO.write(':SYSTem:GTLocal') FlexOTO.close()