Troubleshooting
FlexOTO Instance:
                                                Stations
                                            Use FlexOTO's Troubleshooting mode to locate issues such as:
- DCA-M cannot lock on the signal, and
- Measurement results are questionable.
Troubleshooting mode temporarily disables FlexOTO and launches FlexDCA. This allows you to investigate and change FlexDCA's settings without having to exit FlexOTO.
To use Troubleshoot mode:
- Select a Job ID line in FlexOTO's Results table that you want to investigate.
- Click the Troubleshoot button. The following notice is displayed at the top of FlexOTO.
- FlexOTO automatically opens the FlexDCA application and displays the optical path for the selected Job ID's Fixture / Lane to the DCA-M's input channel.
- While in FlexDCA, you can perform tasks such as:
- Observe the waveform.
- View FlexDCA's N109x Setup dialog or N107x Setup dialog. Click the CDR tile along FlexDCA's bottom edge.
- Investigate the basic measurement settings. Click Measure > Configure Basic Measurements.
- Investigate the PAM-N Analysis setup settings for the TDECQ measurement. In Eye/Mask mode, click on the PAM vertical toolbar and click PAM Setup. Click the TDECQ Configuration tab.
- When your finished with Troubleshoot mode, view the FlexOTO application (press Alt-Tab).
- Click the Exit Troubleshooting button as shown in this screen capture.
                                                     
                                                
                                                     
                                                
 
                                                
                                                     
                                                
Additional Resources
While a Job ID is selected, click on the following buttons located next FlexOTO's Troubleshoot button:
- Details to view the measurement presets used: CDR Preset, TDECQ Meas Preset, and TDECQ EQ Preset.
- View to view see the waveform's eye diagram.
- Save to save a zip file that includes the following information. Be sure to select option for the selected Job ID.
- An eye diagram
- FlexDCA compatible waveform file (.wfmx)
- Text file (.csv) of results data
- Metadata text file (.txt) of setup information