:DISK:RESPonse:SAVE
Command Syntax
:DISK:RESPonse:SAVE "filename.rspx"
Description
Saves a FlexPLL Response file with the indicted filename (.rspx). After the Response file is saved, the file can be reloaded into one of four Response Memories using the :RMEMory:FILE:LOAD command. Response files include the following information:
- Source's Jitter settings
- Receiver's Clock Recovery settings
- JTF plot, JTF model plot , and OJTF model plot
By default, the files are saved in the user-data \Responses folder.
C:\Users\user\Documents\Keysight\FlexPLL>\Responses
Response files must have the extension .rspx. If you do not specify an extension or use a different extension, FlexPLL may not recognize the file as a Response file and you may have trouble saving or finding the file.