:RMEMory:FILE:LOAD
Flex Apps:
FlexPLL
Command Syntax
:RMEMory{1:4}:FILE:LOAD
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3.
Description
Loads the selected Response file (.rspx) into the specified response waveform memory. Use the :RMEMory:FILE:NAME command to specify the name of the file to load. Use the :RMEMory:DISPLay command to display the Response Memory's plots. JTF Response files can also be saved using the :DISK:RESPonse:SAVe command.
Example Command
:RMEMory2:FILE:LOAD