:DISK:SETup:RECall:HCONfig
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
Command Syntax
:DISK:SETup:RECall:HCONfig {ON | OFF}
Query Syntax
:DISK:SETup:RECall:HCONfig?
Description
Enables (ON) or disables (OFF) the loading of extended module configurations when a FlexPLL setup file is opened an using the :DISK:SETup:RECall command. Extended module configurations are always saved with a setup file.