:DISK:SETup:SAVE
Command Syntax
:DISK:SETup:SAVE "filename.setx"
Description
Saves a FlexPLL state setup file with the indicted filename (*.setx). Setup files can be reloaded into FlexPLL using the :DISK:SETup:RECall command. When the application state setup file is re-loaded into the application, the file restores all FlexPLL's settings to those in place at the time that the file was saved.
When you save a setup, the saved settings include:
- N1060A, 81160A, M8000-series, and DCA-M module configurations
- JTF graph scaling
- Display setup
By default, the files are saved in the user data \Setups folder.
C:\Users\user\Documents\Keysight\FlexPLL\Setups
Setup files must have the extension .setx. If you do not specify an extension or use a different extension, FlexPLL may not recognize the file as a setup file and you may have trouble saving or finding the setup file.