:DISK:SIMage:INVert
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
Command Syntax
:DISK:SIMage:INVert {ON | OFF}
Query Syntax
:DISK:SIMage:INVert?
Query Response
{1 | 0}
Description
Turns on and off the inversion the graticule area's background color on a saved image file. When on, an inverted image will be captured and saved into a file by the :DISK:SIMage:SAVE command. The entire application window is saved with the graticule black upon a white background. The waveform colors remain unchanged.