:DISK:SIMage:MONochrome
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
Command Syntax
:DISK:SIMage:MONochrome {ON | OFF | 1 | 0}
Query Syntax
:DISK:SIMage:MONochrome?
Query Response
{1 | 0}
Description
Turns monochrome screen capture on and off when using the :DISK:SIMage:SAVE command. When on, a black and white image will be captured and saved into a file by the :DISK:SIMage:FNAMe command. Selecting monochrome automatically inverts the graticule area's background color.