:MEASure:RESPonse:PFRequency?
Flex Apps:
FlexPLL
Query Syntax
:MEASure:RESPonse:PFRequency?
Description
Returns the frequency for the JTF model waveform's Peaking Frequency measurement. This is the frequency at the maximum peaking on the JTF response for a DUT that uses a 2nd Order PLL. The following figure shows a simplified JTF response with peaking and the corresponding damping on the OJTF response.
When Peaking is selected in the results table, annotation is placed on the graph marking the location of the measurement.
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:RESPonse:PFRequency:STATus?')):
measurement = Flex.query(':MEASure:RESPonse:PFRequency?')
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.
Requires FlexPLL revision A.07.00 and above.