:MEASure:RESPonse:PFRequency:STATus:REASon?
Flex Apps:
FlexPLL
Query Syntax
:MEASure:RESPonse:PFRequency:STATus:REASon?
Description
Returns a string that explains the reason for a failed :MEASure:RESPonse:PFRequency measurement. If the measurement was successful, a null string is returned. Use the :MEASure:RESPonse:PFRequency:STATus? query to determine if the measurement has failed.
Requires FlexPLL revision A.07.00 and above.