:MEASure:RESPonse:PLLModel:FZERo?
Flex Apps:
FlexPLL
Query Syntax
:MEASure:RESPonse:PLLModel:FZERo?
Description
Returns the JTF model waveform's fZero measurement which locates a single frequency in the JTF model where gain decreases. Similar to this is the FPole measurement (:MEASure:RESPonse:PLLModel:FPOLe?) that locates a single frequency in the JTF model where gain increases. A Type 2 PLL by definition has only one pole.
with Zero, Pole, and Gain Frequencies
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:RESPonse:PLLModel:FZERo:STATus?')):
measurement = Flex.query(':MEASure:RESPonse:PLLModel:FZERo?')
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.