:MEASure:RESPonse:PLLModel:FZERo:STATus?
Flex Apps:
FlexPLL
Query Syntax
:MEASure:RESPonse:PLLModel:FZERo:STATus?
Description
Queries the status of the :MEASure:RESPonse:PLLModel:FZERo measurement. Use the :MEASure:RESPonse:PLLModel:FZERo:STATus:REASon? child query to determine the reason for a invalid or questionable measurement.
The query response is:
{CORR | INV | QUES}
CORR- The measurement result is correct.
INV- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
QUES- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.