:RMEMory:FLATness:MEASure:DISPlay

Flex Apps:
FlexPLL

Command Syntax

:RMEMory{1:4}:FLATness:MEASure:DISPlay {ON | OFF}

Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:PLLModel:MEASure:DISPlay.

Query Syntax

:RMEMory{1:4}:FLATness:MEASure:DISPlay?

Query Response

{1 | 0}

Description

Turns on or off the display of the Average, Minimum, and Maximum measurements for the all displayed Memories in the results table. If the :RMEMory:DISPlay command is set to OFF, this command will not be able to display the measurements and the measurements cannot be returned. To return the measurements, use the following commands located in the :MEASure subsystem:

Display Flatness Measurement's Effect on Measurements Displayed
Measurement :RMEMory:FLATness:MEAS:DISP
Command
OFF ON
Maximum ■
Minimum ■
Average ■
Bandwidth ■ ■
Peaking ■ ■
Gain Frequency 1 ■ ■
Zero Frequency 1 ■ ■
Pole Frequency 1 ■ ■
Footnotes:
1. Displayed if :RMEMory:PLLModel:MEASure:DISPlay command ON.

Example Command

:RMEMory2:FLATness:MEASure:DISPlay ON