:RMEMory:DISPlay
Flex Apps:
FlexPLL
Command Syntax
:RMEMory{1:4}:DISPlay {ON | OFF}
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:DISPlay.
Query Syntax
:RMEMory{1:4}:DISPlay?
Query Response
{1 | 0}
Description
Turns the display of the selected response Memory plots on the JTF graph on or off. This setting controls all three response Memory plots: JTF, OJTF, and JTF model. Use the :RMEMory:AVAilable? query to determine if the indicated memory has data in it.
Turns the display of the selected response Memory measurements and plots on the JTF graph on or off. If this command is OFF, the state of the :RMEMory:DISPlay:MODel:JTF, :RMEMory:DISPlay:MODel:OJTF, and :RMEMory:DISPlay:MODel:MEASure child commands will have no effect.
Example Command
:RMEMory2:DISPlay ON