IGBT: Ic-Vge for Expander Test
Measures Ic-Vge transfer characteristics for IGBT devices with multiple Vce values.
Used with:
-
B1506A: IGBT DUT
- B1505A: IGBT DUT, IV test type
- This test requires Ic-Vge PD1000A.xtdconfiguration file. See Install PD1000A Configuration Files for more information.
- If the data sheet lists a maximum test limit for a parameter, use that value.
- If there is no maximum test limit, use a typical value.
See also Setting IV and CV Test Parameters.
Test Schematic
Gate Parameters
Click here for detailed information about each item in the list.
Gate: The SMU connected to Gate terminal, primary sweep voltage output. Select Gate SMU from the drop-down menu.
VgeStart (V): The Sweep start voltage for gate pulse bias.
VgeStop (V): The Sweep stop voltage for gate pulse bias.
VgeStep (V): The Sweep step voltage for gate pulse bias.
IgLimit (A): The Upper limit of gate current.
VgeBase (V): The Gate pulse baseline voltage.
VgeWidth (s): The Gate pulse width (in seconds).
VgeDelay (s): The Gate pulse delay time (in seconds).
Emitter: The GNDU:GND connected to Emitter terminal. This field cannot be changed.
Gate Resistance: Specify the desired Gate Resistance for the device, either 0 (default), 10, 100, or 1000 W.You must set the same Gate Resistance value in two places: 1) in the parameters for this test; and 2) in the EasyEXPERT software for your B1505A or B1506A power analyzer. See Additional IV and CV Test Information.
Collector Parameters
Click here for detailed information about each item in the list.
Collector: The SMU connected to Collector terminal, secondary sweep voltage output. In general, use the Input UHCU for this test.
VceStart (V): The Sweep start voltage for Collector terminal.
VceStop (V): The Sweep stop voltage for Collector terminal.
VceStep (V): The Sweep step voltage for Collector terminal.
IcLimit (A): The Upper limit of collector current.
VceBase (V): The Collector pulse base line voltage.
VceWidth (s): The Collector pulse width.
VceDelay (s): The Collector pulse delay time.
PulsePeriodMode (s): The Pulse period mode, AUTO or MANUAL.
ManualPulsePeriod (s): The Pulse period, effective if PulsePeriodMode = MANUAL.
MeasTime (s): The Actual measurement time for a pulse period.
PulseAvgCnt: The Pulse averaging count.