FET: Id-Vgs for Expander Test
Performs an Id-Vgs measurement by using UHCU, HVMCU and UHVU while the voltage drop at the output resistance of expanders is compensated to make Vds constant.
Used with:
-
B1506A: FET DUT
- B1505A: FET DUT, IV test type
- This test requires Id-Vgs PD1000A.xtdconfiguration file. See Install PD1000A Configuration Files for more information.
- If the data sheet lists a maximum test limit for a parameter, use that value.
- If there is no maximum test limit, use a typical value.
See also Setting IV and CV Test Parameters.
Test Schematic
Gate Parameters
Click here for detailed information about each item in the list.
Gate: The SMU connected to Gate terminal, primary sweep voltage output. Select Gate SMU from the drop-down menu.
VgsStart (V): The Sweep start voltage for gate pulse bias.
VgsStop (V): The Sweep stop voltage for gate pulse bias.
VgsStep (V): The Sweep step voltage for gate pulse bias.
IgLimit (A): The upper limit of gate current.
VgsBase (V): The Gate pulse baseline voltage.
VgsWidth (s): The Gate pulse width.
VgsDelay (s): The Gate pulse delay time.
Source: The GNDU:GND connected to Source terminal. This field cannot be changed.
Gate Resistance: Gate Resistance: Specify the desired Gate Resistance for the device, either 0 (default), 10, 100, or 1000 W.You must set the same Gate Resistance value in two places: 1) in the parameters for this test; and 2) in the EasyEXPERT software for your B1505A or B1506A power analyzer. See Additional IV and CV Test Information.
Drain Parameters
Click here for detailed information about each item in the list.
Drain: The SMU connected to Drain terminal, secondary sweep voltage output. In general, use the Input UHCU for this test.
Vds (V): The Drain voltage.
Vds (V): The Drain voltage.
Vds (V): The Drain voltage.
IdLimit (A): The Upper limit of drain current.
VdsBase (V): The Drain pulse base line voltage.
VdsWidth (s): The Drain pulse width.
VdsDelay (s): The Drain pulse delay time.
PulsePeriodMode: The Pulse period mode, AUTO or MANUAL. (If you choose MANUAL, you must also set the ManualPulsePeriod parameter.)
ManualPulsePeriod (s): The Pulse period. Use this parameter only when you have selected PulsePeriodMode = MANUAL.
PulseWidth (s): The Pulse width.
MeasTime (s): The Actual measurement time for a pulse period.
PulseAvgCnt: The Pulse averaging count.