IGpibIntfc::AddressingState
Description
Shows whether the specified GPIB interface is currently addressed to talk or listen, or is not addressed.
VB Prototype
Dim value As GPIBAddressState
                                            value = object.AddressingState
                                        
C++ Prototype
HRESULT get_AddressingState(
                                        
  GPIBAddressState* AddressingState
);
		
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, AddressingState, ATNState, DevStatusByte, CICState, HS488CBLLength, NDACState, PrimaryAddress, RENState, SecondaryAddress, SRQState, SysControlState, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, Command, ControlATN, ControlREN, PassControl, SendIFC, IGpibIntfc Overview