IGpibIntfc::OptionString
Description
The option string corresponding to the current state of the resource.
See The Option String for more information on the option string property.
VB Prototype
Dim value As String
                                            value = object.OptionString
                                        
C++ Prototype
HRESULT get_OptionString(
                                        
  BSTR* OptionString
);
		
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, AddressingState, ATNState, DevStatusByte, CICState, HS488CBLLength, NDACState, PrimaryAddress, RENState, SecondaryAddress, SRQState, SysControlState, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, Command, ControlATN, ControlREN, PassControl, SendIFC, IGpibIntfc Overview