IGpibIntfc::HardwareInterfaceNumber
Description
The board number of the hardware interface.
VB Prototype
Dim value As Short
                                            value = object.HardwareInterfaceNumber
                                        
C++ Prototype
HRESULT get_HardwareInterfaceNumber(
                                        
  short* HardwareInterfaceNumber
);
		
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, AddressingState, ATNState, DevStatusByte, CICState, HS488CBLLength, NDACState, PrimaryAddress, RENState, SecondaryAddress, SRQState, SysControlState, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, Command, ControlATN, ControlREN, PassControl, SendIFC, IGpibIntfc Overview