IGpibIntfc::SysControlState
Description
Shows whether the specified GPIB interface is currently the system controller. In some implementations, this attribute may be modified only through a configuration utility. On these systems, this attribute is read only (RO).
VB Prototype
Dim value As Boolean
                                            value = object.SysControlState
                                        
object.SysControlState = value 
                                        
C++ Prototype
HRESULT get_SysControlState(
                                        
  VARIANT_BOOL* SysControlState
);
		
HRESULT put_SysControlState(
                                        
  VARIANT_BOOL SysControlState
);
		
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, AddressingState, ATNState, DevStatusByte, CICState, HS488CBLLength, NDACState, PrimaryAddress, RENState, SecondaryAddress, SRQState, SysControlState, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, Command, ControlATN, ControlREN, PassControl, SendIFC, IGpibIntfc Overview