IGpibIntfc::Command
Description
Writes GPIB command bytes on the bus.
This operation attempts to write count number of bytes of GPIB commands to the interface bus associated with the session object. This operation returns only when the transfer terminates.
VB Prototype
value As 
				Long = Command(
                                        
  buffer As SAFEARRAY(BYTE),
  count As Long
)
	
C++ Prototype
HRESULT Command(
                                        
  SAFEARRAY(BYTE)* buffer,
  long count,
  long* pRetCount
);
	
Parameters
buffer
count
pRetCount
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, AddressingState, ATNState, DevStatusByte, CICState, HS488CBLLength, NDACState, PrimaryAddress, RENState, SecondaryAddress, SRQState, SysControlState, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, Command, ControlATN, ControlREN, PassControl, SendIFC, IGpibIntfc Overview