IGpibIntfcMessage::AssertTrigger
Description
Asserts a software or hardware trigger dependent on the interface type. For a GPIB device, the device is addressed to listen, and then the GPIB GET command is sent.
VB Prototype
AssertTrigger(
protocol As TriggerProtocol ' Optional Parameter
)
C++ Prototype
HRESULT AssertTrigger(
TriggerProtocol protocol
);
Parameters
protocol
[Optional in Visual Basic] Trigger protocol to use during assertion.
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Read, ReadString, Write, WriteString, IGpibIntfcMessage Overview