IGpibIntfcMessage::SendEndEnabled
Description
Enables/disables sending the END signal on the last byte of a write.
VB Prototype
Dim value As Boolean
value = object.SendEndEnabled
object.SendEndEnabled = value
C++ Prototype
HRESULT get_SendEndEnabled(
VARIANT_BOOL* SendEndEnabled
);
HRESULT put_SendEndEnabled(
VARIANT_BOOL SendEndEnabled
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Read, ReadString, Write, WriteString, IGpibIntfcMessage Overview