IGpibIntfcMessage::GetAttribute

Description

Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces.

VB Prototype

value As Variant = GetAttribute(
  attribute As Long
)

C++ Prototype

HRESULT GetAttribute(
  long attribute,
  VARIANT* pAttrState
);

Parameters

attribute

The attribute type to retrieve.

pAttrState

The value of the attribute.

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Read, ReadString, Write, WriteString, IGpibIntfcMessage Overview