IGpibIntfcMessage::TerminationCharacter
Description
The ASCII character used to end reading. Setting this property does not enable/disable the sending of this character; that is done by the TerminationCharacterEnabled property. The default character in most VISA implementations and most instruments is ASCII code 10 (linefeed).
VB Prototype
Dim value As Byte
value = object.TerminationCharacter
object.TerminationCharacter = value
C++ Prototype
HRESULT get_TerminationCharacter(
BYTE* TerminationCharacter
);
HRESULT put_TerminationCharacter(
BYTE TerminationCharacter
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Read, ReadString, Write, WriteString, IGpibIntfcMessage Overview