IGpibIntfcMessage::TerminationCharacterEnabled

Description

Enables/disables ending reads upon reception of the termination character. Enabling this property does not cause the termination character to be appended to writes.

VB Prototype

Dim value As Boolean
value = object.TerminationCharacterEnabled

object.TerminationCharacterEnabled = value

C++ Prototype

HRESULT get_TerminationCharacterEnabled(
  VARIANT_BOOL* TerminationCharacterEnabled
);

HRESULT put_TerminationCharacterEnabled(
  VARIANT_BOOL TerminationCharacterEnabled
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Read, ReadString, Write, WriteString, IGpibIntfcMessage Overview