IHislipInstr2::LastStatus
Description
The return value from the last method call of this session. This property may be useful in Visual Basic, where positive return values, such as warnings and other non-error return values, cannot be retrieved.
See the Return Values page for a list of positive return values.
VB Prototype
Dim value As HRESULT
                                            value = object.LastStatus
                                        
C++ Prototype
HRESULT get_LastStatus(
                                        
  HRESULT* LastStatus
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, EncryptionEnabled, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite, UnlockRsrc, IHislipInstr2 Overview