IHislipInstr2::ProtocolVersion

Description

Returns the negotiated HiSLIP protocol version.

VB Prototype

Dim value As Long
value = object.ProtocolVersion

C++ Prototype

HRESULT get_ProtocolVersion(
  long* ProtocolVersion
);

Return Value

Refer to the table of return codes.

See Also

Address, Close, ComponentVersion, ControlREN, DeviceName, EncryptionEnabled, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite, UnlockRsrc, IHislipInstr2 Overview