IHislipInstr2::MaxMessage
Description
Returns or sets the HiSLIP maximum message size in kbytes (1024 bytes).
VB Prototype
Dim value As Long
                                            
                                            value = object.MaxMessage
                                        
object.MaxMessage = value 
                                        
C++ Prototype
HRESULT get_MaxMessage(
                                        
  long* MaxMessage
);
		
HRESULT put_MaxMessage(
                                        
  long MaxMessage
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, EncryptionEnabled, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite, UnlockRsrc, IHislipInstr2 Overview