IHislipInstr2::ServerCertificateExpirationDate
Description
Returns the expiration date of the server certificate.
VB Prototype
Dim value As String
                                            value = object.ServerCertificateExpirationDate
                                        
C++ Prototype
HRESULT get_ServerCertificateExpirationDate(
                                        
  BSTR* ServerCertificateExpirationDate
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, EncryptionEnabled, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite, UnlockRsrc, IHislipInstr2 Overview