IHislipInstr2::TlsCipherSuite
Description
Returns the TLS cipher suite used by the connection.
VB Prototype
Dim value As String
                                            value = object.TlsCipherSuite
                                        
C++ Prototype
HRESULT get_TlsCipherSuite(
                                        
  BSTR* TlsCipherSuite
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, EncryptionEnabled, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite, UnlockRsrc, IHislipInstr2 Overview