ITcpipInstr2::DeviceName
Description
Specifies the LAN device name used by the VXI-11 protocol during connection.
VB Prototype
Dim value As String
value = object.DeviceName
C++ Prototype
HRESULT get_DeviceName(
BSTR* DeviceName
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, DeviceName, GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, OptionString, ProgID, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, , ITcpipInstr2 Overview