ITcplipInstr2::ServerCertificateSubjectName
Description
Returns the subject name of the server certificate.
VB Prototype
Dim value As String
                                            value = object.ServerCertificateSubjectName
                                        
C++ Prototype
HRESULT get_ServerCertificateSubjectName(
                                        
  BSTR* ServerCertificateSubjectName
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, DeviceName, GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, OptionString, ProgID, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, , ITcpipInstr2 Overview