ITcpipInstr2::Timeout
Description
The I/O timeout in milliseconds for I/O communication on this resource session.
VB Prototype
Dim value As L
ongvalue = object.Timeout
object.Timeout = value
C++ Prototype
HRESULT get_Timeout(
long* Timeout
);
HRESULT put_Timeout(
long Timeout
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, DeviceName, GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, OptionString, ProgID, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, , ITcpipInstr2 Overview