ITcpipInstr2::ServerCertificateIssuerName
Description
Returns the issuer name of the server certificate.
VB Prototype
Dim value As String
                                            value = object.ServerCertificateIssuerName
                                        
C++ Prototype
HRESULT get_ServerCertificateIssuerName(
                                        
  BSTR* ServerCertificateIssuerName
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, DeviceName, GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, OptionString, ProgID, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, , ITcpipInstr2 Overview