ITcpipInstr2::ServerCertificateIsPerpetual

Description

Returns a value indicating whether the server certificate is perpetual or not.

VB Prototype

Dim value As Boolean
value = object.ServerCertificateIsPerpetual

C++ Prototype

HRESULT get_ServerCertificateIsPerpetual(
  VARIANT_BOOL* ServerCertificateIsPerpetual
);

Return Value

Refer to the table of return codes.

See Also

Address, Close, ComponentVersion, DeviceName, GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, OptionString, ProgID, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, , ITcpipInstr2 Overview