ITcpipSocket::Address
Description
The TCPIP address of the device to which the session is connected. This string is formatted in dot-notation.
VB Prototype
Dim value As String
                                            value = object.Address
                                        
C++ Prototype
HRESULT get_Address(
                                        
  BSTR* Address
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, Address, HostName, KeepAlive, NoDelay, Port, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ITcpipSocket Overview