ITcpipSocket::NoDelay
Description
The Nagle algorithm is disabled when this attribute is enabled (and vice versa). The Nagle algorithm improves network performance by buffering send data until a full-size packet can be sent. This attribute is enabled by default in VISA to verify that synchronous writes get flushed immediately.
VB Prototype
Dim value As Boolean
                                            value = object.NoDelay
                                        
object.NoDelay = value 
                                        
C++ Prototype
HRESULT get_NoDelay(
                                        
  VARIANT_BOOL* NoDelay
);
		
HRESULT put_NoDelay(
                                        
  VARIANT_BOOL NoDelay
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, Address, HostName, KeepAlive, NoDelay, Port, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ITcpipSocket Overview