ITcpipSocket::SoftwareManufacturerName
Description
The name of the vendor of this software component.
VB Prototype
Dim value As String
                                            value = object.SoftwareManufacturerName
                                        
C++ Prototype
HRESULT get_SoftwareManufacturerName(
                                        
  BSTR* SoftwareManufacturerName
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, Address, HostName, KeepAlive, NoDelay, Port, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ITcpipSocket Overview