ITcpipSocket::Flush
Description
Manually flushes the read and write buffers associated with TCPIP SOCKET interfaces.
VB Prototype
Flush(
mask As BufferMask, ' Optional Parameter
discard As Boolean ' Optional Parameter
)
C++ Prototype
HRESULT Flush(
BufferMask mask,
VARIANT_BOOL discard
);
Parameters
mask
[Optional in Visual Basic] Which serial buffer to resize, the in buffer, the out buffer, or both.
discard
[Optional in Visual Basic] Specifies whether to due a discard of the data or perform I/O to the device.
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, Address, HostName, KeepAlive, NoDelay, Port, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ITcpipSocket Overview