ITcpipSocket::HostName

Description

Specifies the host name of the device. If no host name is available, this attribute returns an empty string.

VB Prototype

Dim value As String
value = object.HostName

C++ Prototype

HRESULT get_HostName(
  BSTR* HostName
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, Address, HostName, KeepAlive, NoDelay, Port, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ITcpipSocket Overview