IUsb::Close

Description

Closes the resource. Sending the resource's COM object's reference count to zero (and thus destroying the object) also executes a close, but this method may be useful for environments with garbage collection or other facilities that make object lifetimes non-deterministic.

VB Prototype

Close(
)

C++ Prototype

HRESULT Close(
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, ManufacturerID, ManufacturerName, ModelCode, ModelName, Is4882Compliant, UsbSerialNumber, UsbInterfaceNumber, UsbProtocol, MaximumInterruptSize, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, ControlOut, ControlIn, IUsb Overview