IUsb::UsbProtocol
Description
Specifies the USB protocol number.
VB Prototype
Dim value As Short
value = object.UsbProtocol
C++ Prototype
HRESULT get_UsbProtocol(
short* UsbProtocol
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, ManufacturerID, ManufacturerName, ModelCode, ModelName, Is4882Compliant, UsbSerialNumber, UsbInterfaceNumber, UsbProtocol, MaximumInterruptSize, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, ControlOut, ControlIn, IUsb Overview