IUsb::MaximumInterruptSize

Description

Specifies the maximum number of bytes that this USB device will send on the interrupt IN pipe. The default value is the same as the maximum packet size of the interrupt IN pipe.

VB Prototype

Dim value As Short
value = object.MaximumInterruptSize

object.MaximumInterruptSize = value

C++ Prototype

HRESULT get_MaximumInterruptSize(
  short* MaximumInterruptSize
);

HRESULT put_MaximumInterruptSize(
  short MaximumInterruptSize
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, ManufacturerID, ManufacturerName, ModelCode, ModelName, Is4882Compliant, UsbSerialNumber, UsbInterfaceNumber, UsbProtocol, MaximumInterruptSize, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, ControlOut, ControlIn, IUsb Overview