IUsb::UsbSerialNumber
Description
The serial number of the USB instrument. The value of this attribute should be used for display purposes only and not for programmatic decisions.
VB Prototype
Dim value As String
value = object.UsbSerialNumber
C++ Prototype
HRESULT get_UsbSerialNumber(
BSTR* UsbSerialNumber
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, ManufacturerID, ManufacturerName, ModelCode, ModelName, Is4882Compliant, UsbSerialNumber, UsbInterfaceNumber, UsbProtocol, MaximumInterruptSize, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, ControlOut, ControlIn, IUsb Overview