IUsb::ProgID

Description

The programmatic ID that can be used by COM to create this object.

VB Prototype

Dim value As String
value = object.ProgID

C++ Prototype

HRESULT get_ProgID(
  BSTR* ProgID
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, ManufacturerID, ManufacturerName, ModelCode, ModelName, Is4882Compliant, UsbSerialNumber, UsbInterfaceNumber, UsbProtocol, MaximumInterruptSize, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, ControlOut, ControlIn, IUsb Overview