IGpibIntfc::CICState
Description
Shows whether the specified GPIB interface is currently CIC (controller in charge).
VB Prototype
Dim value As Boolean
value = object.CICState
C++ Prototype
HRESULT get_CICState(
VARIANT_BOOL* CICState
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, AddressingState, ATNState, DevStatusByte, CICState, HS488CBLLength, NDACState, PrimaryAddress, RENState, SecondaryAddress, SRQState, SysControlState, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, Command, ControlATN, ControlREN, PassControl, SendIFC, IGpibIntfc Overview