IGpibIntfc::SecondaryAddress
Description
Secondary address of the local GPIB controller used by the given session.
VB Prototype
Dim value As Short
value = object.SecondaryAddress
object.SecondaryAddress = value
C++ Prototype
HRESULT get_SecondaryAddress(
short* SecondaryAddress
);
HRESULT put_SecondaryAddress(
short SecondaryAddress
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, AddressingState, ATNState, DevStatusByte, CICState, HS488CBLLength, NDACState, PrimaryAddress, RENState, SecondaryAddress, SRQState, SysControlState, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, Command, ControlATN, ControlREN, PassControl, SendIFC, IGpibIntfc Overview